FUTEK .NET API Documentation
FUTEK_USB_DLL Assembly / FUTEK_USB_DLL Namespace / USB_DLL Class / Get_Average_Setting Method


In This Topic
    Get_Average_Setting Method
    In This Topic
    Get_Average_Setting is a Function that returns a value representing the Average Setting.
    Syntax
    'Declaration
     
    
    Public Function Get_Average_Setting( _
       ByVal DeviceHandle As IntPtr, _
       Optional ByVal ChannelNumber As Byte _
    ) As String
    'Usage
     
    
    Dim instance As USB_DLL
    Dim DeviceHandle As IntPtr
    Dim ChannelNumber As Byte
    Dim value As String
     
    value = instance.Get_Average_Setting(DeviceHandle, ChannelNumber)
    public string Get_Average_Setting( 
       IntPtr DeviceHandle,
       byte ChannelNumber
    )

    Parameters

    DeviceHandle
    ChannelNumber

    Return Value

    If successful, The Return Value will be:

    For USB100 and USB200:

    Return Value = "Error"; There is no Average Setting for this Type of Board

    For USB110, USB210, USB220, USB230:

    Averaging Method: Disable Average

    Return Value = (00H); Number of Samples to Average = 2

    Return Value = (01H); Number of Samples to Average = 4

    Return Value = (02H); Number of Samples to Average = 8

    Return Value = (03H); Number of Samples to Average = 16

    Return Value = (04H); Number of Samples to Average = 32

    Return Value = (05H); Number of Samples to Average = 64

    Return Value = (06H); Number of Samples to Average = 128

    Return Value = (07H); Number of Samples to Average = 256

    Averaging Method: Moving Average

    Return Value = (10H); Number of Samples to Average = 2

    Return Value = (11H); Number of Samples to Average = 4

    Return Value = (12H); Number of Samples to Average = 8

    Return Value = (13H); Number of Samples to Average = 16

    Return Value = (14H); Number of Samples to Average = 32

    Return Value = (15H); Number of Samples to Average = 64

    Return Value = (16H); Number of Samples to Average = 128

    Return Value = (17H); Number of Samples to Average = 256

    Averaging Method: Mean Average

    Return Value = (20H); Number of Samples to Average = 2

    Return Value = (21H); Number of Samples to Average = 4

    Return Value = (22H); Number of Samples to Average = 8

    Return Value = (23H); Number of Samples to Average = 16

    Return Value = (24H); Number of Samples to Average = 32

    Return Value = (25H); Number of Samples to Average = 64

    Return Value = (26H); Number of Samples to Average = 128

    Return Value = (27H); Number of Samples to Average = 256

    If Unsuccessful, the Return Value will be:

    Return Value = "Error"; An Error occured when attempting to Get_Average_Setting

    Frameworks
    Product Versions
    .NET net10.0
    .NET Framework net48
    See Also