'DeclarationPublic Function Get_Baud_Rate( _ ByVal DeviceHandle As IntPtr, _ Optional ByVal ChannelNumber As Byte _ ) As String
'UsageDim instance As USB_DLL Dim DeviceHandle As IntPtr Dim ChannelNumber As Byte Dim value As String value = instance.Get_Baud_Rate(DeviceHandle, ChannelNumber)
public string Get_Baud_Rate( IntPtr DeviceHandle, byte ChannelNumber )
Parameters
- DeviceHandle
- ChannelNumber
Return Value
If successful, The Return Value will be:
Return Value = Number between 0 and 3;
If Unsuccessful, the Return Value will be:
Return Value = "Error"; An Error occured when attempting to Get_Baud_Rate