FUTEK .NET API Documentation
FUTEK_USB_DLL Assembly / FUTEK_USB_DLL Namespace / USB_DLL Class / Get_Display_Page Method
Type: System.IntPtr
The handle associated with the USB device.


In This Topic
    Get_Display_Page Method
    In This Topic
    Gets the display page from the USB device.
    Syntax
    'Declaration
     
    
    Public Function Get_Display_Page( _
       ByVal DeviceHandle As IntPtr _
    ) As String
    'Usage
     
    
    Dim instance As USB_DLL
    Dim DeviceHandle As IntPtr
    Dim value As String
     
    value = instance.Get_Display_Page(DeviceHandle)
    public string Get_Display_Page( 
       IntPtr DeviceHandle
    )

    Parameters

    DeviceHandle
    Type: System.IntPtr
    The handle associated with the USB device.

    Return Value

    Type: System.String
    A value equal to 0; otherwise Error
    Remarks
    This function assigns a string of data for each line of the LCD to the following properties: LCDLine1, LCDLine2, LCDLine3 and LCDLine4.
    This function assigns a string of data containing all four lines of the LCD to the following property: DisplayPage.
    Frameworks
    Product Versions
    .NET net10.0
    .NET Framework net48
    See Also