'DeclarationPublic Function Get_Enabled_Channels( _ ByVal deviceHandle As IntPtr, _ Optional ByVal channelNumber As Byte _ ) As String
'UsageDim instance As USB_DLL Dim deviceHandle As IntPtr Dim channelNumber As Byte Dim value As String value = instance.Get_Enabled_Channels(deviceHandle, channelNumber)
public string Get_Enabled_Channels( IntPtr deviceHandle, byte channelNumber )
Parameters
- deviceHandle
- Type: System.IntPtr
The handle associated with the USB device. - channelNumber
- Type: System.Byte
The channel number associated with the USB device.
Return Value
Type: System.String
A value between 0 and 15; otherwise Error
A value between 0 and 15; otherwise Error