'DeclarationPublic Function Get_Firmware_Month( _ ByVal DeviceHandle As IntPtr _ ) As String
'UsageDim instance As USB_DLL Dim DeviceHandle As IntPtr Dim value As String value = instance.Get_Firmware_Month(DeviceHandle)
public string Get_Firmware_Month( IntPtr DeviceHandle )
Parameters
- DeviceHandle
Return Value
If successful, The Return Value will be:
Return Value = (00H); The Month is Invalid
Return Value = (01H); The Month is January
Return Value = (02H); The Month is February
Return Value = (03H); The Month is March
Return Value = (04H); The Month is April
Return Value = (05H); The Month is May
Return Value = (06H); The Month is June
Return Value = (07H); The Month is July
Return Value = (08H); The Month is August
Return Value = (09H); The Month is September
Return Value = (0AH); The Month is October
Return Value = (0BH); The Month is November
Return Value = (0CH); The Month is December
Return Value = (0DH); The Month is Invalid
Return Value = (0EH); The Month is Invalid
Return Value = (0FH); The Month is Invalid
If Unsuccessful, the Return Value will be:
Return Value = "Error"; An Error occured when attempting to Get_Firmware_Month