'DeclarationPublic Function Get_Firmware_Year( _ ByVal DeviceHandle As IntPtr _ ) As String
'UsageDim instance As USB_DLL Dim DeviceHandle As IntPtr Dim value As String value = instance.Get_Firmware_Year(DeviceHandle)
public string Get_Firmware_Year( IntPtr DeviceHandle )
Parameters
- DeviceHandle
Return Value
If successful, The Return Value will be:
Return Value = (00H); The Year is 2000
Return Value = (01H); The Year is 2001
Return Value = (02H); The Year is 2002
Return Value = (03H); The Year is 2003
Return Value = (04H); The Year is 2004
Return Value = (05H); The Year is 2005
Return Value = (06H); The Year is 2006
Return Value = (07H); The Year is 2007
Return Value = (08H); The Year is 2008
Return Value = (09H); The Year is 2009
Return Value = (0AH); The Year is 2010
Return Value = (0BH); The Year is 2011
Return Value = (0CH); The Year is 2012
Return Value = (0DH); The Year is 2013
Return Value = (0EH); The Year is 2014
Return Value = (0FH); The Year is 2015
If Unsuccessful, the Return Value will be:
Return Value = "Error"; An Error occured when attempting to Get_Firmware_Year