FUTEK .NET API Documentation
FUTEK_USB_DLL Assembly / FUTEK_USB_DLL Namespace / USB_DLL Class / Get_Hardware_Version Method


In This Topic
    Get_Hardware_Version Method
    In This Topic
    Get_Hardware_Version is a Function that returns a value representing the Hardware Version of the USB Device.
    Syntax
    'Declaration
     
    
    Public Function Get_Hardware_Version( _
       ByVal DeviceHandle As IntPtr _
    ) As String
    'Usage
     
    
    Dim instance As USB_DLL
    Dim DeviceHandle As IntPtr
    Dim value As String
     
    value = instance.Get_Hardware_Version(DeviceHandle)
    public string Get_Hardware_Version( 
       IntPtr DeviceHandle
    )

    Parameters

    DeviceHandle

    Return Value

    If successful, The Return Value will be:

    Return Value = (00H to FFH);

    If Unsuccessful, the Return Value will be:

    Return Value = "Error"; An Error occured when attempting to Get_Hardware_Version

    Frameworks
    Product Versions
    .NET net10.0
    .NET Framework net48
    See Also