FUTEK .NET API Documentation
FUTEK_USB_DLL Assembly / FUTEK_USB_DLL Namespace / USB_DLL Class / Get_Source_IP_Address Method


In This Topic
    Get_Source_IP_Address Method
    In This Topic
    Get_Source_IP_Address is a Function that returns a value representing the Source IP Address of the Device.
    Syntax
    'Declaration
     
    
    Public Function Get_Source_IP_Address( _
       ByVal DeviceHandle As IntPtr, _
       Optional ByVal ChannelNumber As Byte _
    ) As String
    'Usage
     
    
    Dim instance As USB_DLL
    Dim DeviceHandle As IntPtr
    Dim ChannelNumber As Byte
    Dim value As String
     
    value = instance.Get_Source_IP_Address(DeviceHandle, ChannelNumber)
    public string Get_Source_IP_Address( 
       IntPtr DeviceHandle,
       byte ChannelNumber
    )

    Parameters

    DeviceHandle
    ChannelNumber

    Return Value

    If successful, The Return Value will be:

    Return Value = 0;

    If Unsuccessful, the Return Value will be:

    Return Value = "Error"; An Error occured when attempting to Get_Source_IP_Address

    Frameworks
    Product Versions
    .NET net10.0
    .NET Framework net48
    See Also