'Declaration
Public Function Get_Type_of_Board( _ ByVal DeviceHandle As IntPtr _ ) As String
'Usage
Dim instance As USB_DLL Dim DeviceHandle As IntPtr Dim value As String value = instance.Get_Type_of_Board(DeviceHandle)
public string Get_Type_of_Board( IntPtr DeviceHandle )
Parameters
- DeviceHandle
Return Value
If successful, The Return Value will be:
Return Value = (00H); The Type of Board is "USB100"
Return Value = (01H); The Type of Board is "USB110"
Return Value = (02H); The Type of Board is "USB210"
Return Value = (03H); The Type of Board is "USB220"
Return Value = (04H); The Type of Board is "USB230"
Return Value = (05H to FFH); The Type of Board is an "Unknown Type of Board"
If Unsuccessful, the Return Value will be:
Return Value = "Error"; An Error occured when attempting to Get_Type_of_Board