'Declaration
Public Function Get_Voltage_Output( _ ByVal DeviceHandle As IntPtr, _ Optional ByVal ChannelNumber As Byte _ ) As String
'Usage
Dim instance As USB_DLL Dim DeviceHandle As IntPtr Dim ChannelNumber As Byte Dim value As String value = instance.Get_Voltage_Output(DeviceHandle, ChannelNumber)
public string Get_Voltage_Output( IntPtr DeviceHandle, byte ChannelNumber )
Parameters
- DeviceHandle
- ChannelNumber
Return Value
If successful, The Return Value will be:
Return Value = Number between 0 and 255;
If Unsuccessful, the Return Value will be:
Return Value = "Error"; An Error occured when attempting to Get_Voltage_Output