'DeclarationPublic Function Normal_Data_Request( _ ByVal DeviceHandle As IntPtr, _ Optional ByVal ChannelNumber As Byte _ ) As String
'UsageDim instance As USB_DLL Dim DeviceHandle As IntPtr Dim ChannelNumber As Byte Dim value As String value = instance.Normal_Data_Request(DeviceHandle, ChannelNumber)
public string Normal_Data_Request( IntPtr DeviceHandle, byte ChannelNumber )
Parameters
- DeviceHandle
- Type: System.IntPtr
The handle associated with the USB device. - ChannelNumber
- Type: System.Byte
The channel number associated with the USB device.
Return Value
Type: System.String
A value between -16,777,216 and 16,777,215; otherwise Error
A value between -16,777,216 and 16,777,215; otherwise Error