FUTEK .NET API Documentation
FUTEK_USB_DLL Assembly / FUTEK_USB_DLL Namespace / USB_DLL Class / Reset_Board Method
Type: System.IntPtr
The handle associated with the USB device.


In This Topic
    Reset_Board Method
    In This Topic
    Resets the microcontroller.
    Syntax
    'Declaration
     
    
    Public Function Reset_Board( _
       ByVal DeviceHandle As IntPtr _
    ) As String
    'Usage
     
    
    Dim instance As USB_DLL
    Dim DeviceHandle As IntPtr
    Dim value As String
     
    value = instance.Reset_Board(DeviceHandle)
    public string Reset_Board( 
       IntPtr DeviceHandle
    )

    Parameters

    DeviceHandle
    Type: System.IntPtr
    The handle associated with the USB device.

    Return Value

    Type: System.String
    A value equal to 0; otherwise Error
    Remarks
    This function may take several seconds to respond.
    Frameworks
    Product Versions
    .NET net10.0
    .NET Framework net48
    See Also