'DeclarationPublic Function Restore_Back_Up( _ ByVal DeviceHandle As IntPtr, _ ByVal DestinationPageNumber As Integer, _ ByVal SourcePageNumber As Integer _ ) As String
'UsageDim instance As USB_DLL Dim DeviceHandle As IntPtr Dim DestinationPageNumber As Integer Dim SourcePageNumber As Integer Dim value As String value = instance.Restore_Back_Up(DeviceHandle, DestinationPageNumber, SourcePageNumber)
public string Restore_Back_Up( IntPtr DeviceHandle, int DestinationPageNumber, int SourcePageNumber )
Parameters
- DeviceHandle
- DestinationPageNumber
- SourcePageNumber
Return Value
If successful:
Return Value = 0
If Unsuccessful, the Return Value will be:
Return Value = "Error"; An Error occured when attempting Restore_Back_Up