FUTEK .NET API Documentation
FUTEK_USB_DLL Assembly / FUTEK_USB_DLL Namespace / USB_DLL Class / Set_Active_Page_Number Method
Type: System.IntPtr
The handle associated with the USB device.
Type: System.Int32
The active page number associated with the USB device.
The value must be between 0 and 7.
Type: System.Byte
The channel number associated with the USB device.


In This Topic
    Set_Active_Page_Number Method
    In This Topic
    Warning: The use of this function can affect the factory calibration of the USB device.
    Sets the active page number stored in the EEPROM of the microcontroller.
    Syntax
    'Declaration
     
    
    Public Function Set_Active_Page_Number( _
       ByVal DeviceHandle As IntPtr, _
       ByVal ActivePageNumber As Integer, _
       Optional ByVal ChannelNumber As Byte _
    ) As String
    'Usage
     
    
    Dim instance As USB_DLL
    Dim DeviceHandle As IntPtr
    Dim ActivePageNumber As Integer
    Dim ChannelNumber As Byte
    Dim value As String
     
    value = instance.Set_Active_Page_Number(DeviceHandle, ActivePageNumber, ChannelNumber)
    public string Set_Active_Page_Number( 
       IntPtr DeviceHandle,
       int ActivePageNumber,
       byte ChannelNumber
    )

    Parameters

    DeviceHandle
    Type: System.IntPtr
    The handle associated with the USB device.
    ActivePageNumber
    Type: System.Int32
    The active page number associated with the USB device.
    The value must be between 0 and 7.
    ChannelNumber
    Type: System.Byte
    The channel number associated with the USB device.

    Return Value

    Type: System.String
    A value equal to 0; otherwise Error
    Remarks
    The ActivePageNumber is a value indicating...
    Frameworks
    Product Versions
    .NET net10.0
    .NET Framework net48
    See Also