'DeclarationPublic Function Set_Active_Sound( _ ByVal DeviceHandle As IntPtr, _ ByVal activeSound As Byte, _ Optional ByVal channelNumber As Byte _ ) As String
'UsageDim instance As USB_DLL Dim DeviceHandle As IntPtr Dim activeSound As Byte Dim channelNumber As Byte Dim value As String value = instance.Set_Active_Sound(DeviceHandle, activeSound, channelNumber)
public string Set_Active_Sound( IntPtr DeviceHandle, byte activeSound, byte channelNumber )
Parameters
- DeviceHandle
- Type: System.IntPtr
The handle associated with the USB device. - activeSound
- Type: System.Byte
The active sound associated with the USB device.
The value must be between 0 and 1. - channelNumber
- Type: System.Byte
The channel number associated with the USB device.
Return Value
Type: System.String
A value equal to 0; otherwise Error
A value equal to 0; otherwise Error