'DeclarationPublic Function Set_Calibration_Mode( _ ByVal DeviceHandle As IntPtr, _ ByVal PotentiometerNumber As Byte, _ ByVal Adjustment As Byte, _ Optional ByVal ChannelNumber As Byte _ ) As String
'UsageDim instance As USB_DLL Dim DeviceHandle As IntPtr Dim PotentiometerNumber As Byte Dim Adjustment As Byte Dim ChannelNumber As Byte Dim value As String value = instance.Set_Calibration_Mode(DeviceHandle, PotentiometerNumber, Adjustment, ChannelNumber)
public string Set_Calibration_Mode( IntPtr DeviceHandle, byte PotentiometerNumber, byte Adjustment, byte ChannelNumber )
Parameters
- DeviceHandle
- Type: System.IntPtr
The handle associated with the USB device. - PotentiometerNumber
- Type: System.Byte
The potentiometer number associated with the USB device. - Adjustment
- Type: System.Byte
The adjustment associated with the USB device. - ChannelNumber
- Type: System.Byte
The channel number associated with the USB device.
Return Value
Type: System.String
A value equal to 0; otherwise Error
A value equal to 0; otherwise Error