'DeclarationPublic Function Set_Calibration_Register( _ ByVal DeviceHandle As IntPtr, _ ByVal Register As Byte, _ ByVal HighByte As Byte, _ ByVal LowByte As Byte, _ Optional ByVal ChannelNumber As Byte _ ) As String
Parameters
- DeviceHandle
- Type: System.IntPtr
The handle associated with the USB device. - Register
- Type: System.Byte
The calibration register associated with the USB device.
The value must be between 0 and 19. - HighByte
- Type: System.Byte
The high byte of data to assign the calibration register. - LowByte
- Type: System.Byte
The low byte of data to assign the calibration register. - ChannelNumber
- Type: System.Byte
The channel number associated with the USB device.
Return Value
Type: System.String
A value equal to 0; otherwise Error
A value equal to 0; otherwise Error