FUTEK .NET API Documentation
FUTEK_USB_DLL Assembly / FUTEK_USB_DLL Namespace / USB_DLL Class / Set_Channel_Configuration Method
Type: System.IntPtr
The handle associated with the USB device.
Type: System.Byte
The channelConfiguration associated with the USB device.
Type: System.Byte
The channel number associated with the USB device.


In This Topic
    Set_Channel_Configuration Method
    In This Topic
    Warning: The use of this function can affect the factory calibration of the USB device.
    Sets the channel configuration associated with the USB device.
    Syntax
    'Declaration
     
    
    Public Function Set_Channel_Configuration( _
       ByVal deviceHandle As IntPtr, _
       ByVal channelConfiguration As Byte, _
       Optional ByVal channelNumber As Byte _
    ) As String
    'Usage
     
    
    Dim instance As USB_DLL
    Dim deviceHandle As IntPtr
    Dim channelConfiguration As Byte
    Dim channelNumber As Byte
    Dim value As String
     
    value = instance.Set_Channel_Configuration(deviceHandle, channelConfiguration, channelNumber)
    public string Set_Channel_Configuration( 
       IntPtr deviceHandle,
       byte channelConfiguration,
       byte channelNumber
    )

    Parameters

    deviceHandle
    Type: System.IntPtr
    The handle associated with the USB device.
    channelConfiguration
    Type: System.Byte
    The channelConfiguration associated with the USB device.
    channelNumber
    Type: System.Byte
    The channel number associated with the USB device.

    Return Value

    Type: System.String
    A value equal to 0; otherwise Error
    Remarks
    The channelConfiguration can be used to enable or disable each channel and the Active SounD.
    Frameworks
    Product Versions
    .NET net10.0
    .NET Framework net48
    See Also