FUTEK .NET API Documentation
FUTEK_USB_DLL Assembly / FUTEK_USB_DLL Namespace / USB_DLL Class / Set_CrossTalk Method
Type: System.IntPtr
The handle associated with the USB device.
Type: System.Int32
The crosstalk associated with the USB device.
The value must be between 0 and 1.
Type: System.Byte
The channel number associated with the USB device.


In This Topic
    Set_CrossTalk Method
    In This Topic
    Warning: The use of this function can affect the factory calibration of the USB device.
    Sets the crosstalk value stored in the EEPROM of the microcontroller.
    Syntax
    'Declaration
     
    
    Public Function Set_CrossTalk( _
       ByVal DeviceHandle As IntPtr, _
       ByVal CrossTalk As Integer, _
       Optional ByVal ChannelNumber As Byte _
    ) As String
    'Usage
     
    
    Dim instance As USB_DLL
    Dim DeviceHandle As IntPtr
    Dim CrossTalk As Integer
    Dim ChannelNumber As Byte
    Dim value As String
     
    value = instance.Set_CrossTalk(DeviceHandle, CrossTalk, ChannelNumber)

    Parameters

    DeviceHandle
    Type: System.IntPtr
    The handle associated with the USB device.
    CrossTalk
    Type: System.Int32
    The crosstalk associated with the USB device.
    The value must be between 0 and 1.
    ChannelNumber
    Type: System.Byte
    The channel number associated with the USB device.

    Return Value

    Type: System.String
    A value equal to 0; otherwise Error
    Remarks
    The CrossTalk is a value indicating...
    Frameworks
    Product Versions
    .NET net8.0
    .NET Framework net48
    See Also