FUTEK .NET API Documentation
FUTEK_USB_DLL Assembly / FUTEK_USB_DLL Namespace / USB_DLL Class / Set_Destination_Port_Number Method
Type: System.IntPtr
The handle associated with the USB device.
Type: System.Int32
The port number associated with the device.
Type: System.Byte
The channel number associated with the USB device.


In This Topic
    Set_Destination_Port_Number Method
    In This Topic
    Warning: The use of this function can affect the factory calibration of the USB device.
    Sets the destination port number stored in the EEPROM of the microcontroller.
    Syntax
    'Declaration
     
    
    Public Function Set_Destination_Port_Number( _
       ByVal DeviceHandle As IntPtr, _
       ByVal PortNumber As Integer, _
       Optional ByVal ChannelNumber As Byte _
    ) As String
    'Usage
     
    
    Dim instance As USB_DLL
    Dim DeviceHandle As IntPtr
    Dim PortNumber As Integer
    Dim ChannelNumber As Byte
    Dim value As String
     
    value = instance.Set_Destination_Port_Number(DeviceHandle, PortNumber, ChannelNumber)
    public string Set_Destination_Port_Number( 
       IntPtr DeviceHandle,
       int PortNumber,
       byte ChannelNumber
    )

    Parameters

    DeviceHandle
    Type: System.IntPtr
    The handle associated with the USB device.
    PortNumber
    Type: System.Int32
    The port number associated with the device.
    ChannelNumber
    Type: System.Byte
    The channel number associated with the USB device.

    Return Value

    Type: System.String
    A value equal to 0; otherwise Error
    Remarks
    Frameworks
    Product Versions
    .NET net10.0
    .NET Framework net48
    See Also