FUTEK .NET API Documentation
FUTEK_USB_DLL Assembly / FUTEK_USB_DLL Namespace / USB_DLL Class / Set_Enabled_Channels Method
Type: System.IntPtr
The handle associated with the USB device.
Type: System.Byte
The enabled channels associated with the USB device.
The value must be between 0 and 1.
Type: System.Byte
The channel number associated with the USB device.


In This Topic
    Set_Enabled_Channels Method
    In This Topic
    Warning: The use of this function can affect the factory calibration of the USB device.
    Sets the enabled channels stored in the EEPROM of the microcontroller.
    Syntax
    'Declaration
     
    
    Public Function Set_Enabled_Channels( _
       ByVal DeviceHandle As IntPtr, _
       ByVal enabledChannels As Byte, _
       Optional ByVal channelNumber As Byte _
    ) As String
    'Usage
     
    
    Dim instance As USB_DLL
    Dim DeviceHandle As IntPtr
    Dim enabledChannels As Byte
    Dim channelNumber As Byte
    Dim value As String
     
    value = instance.Set_Enabled_Channels(DeviceHandle, enabledChannels, channelNumber)
    public string Set_Enabled_Channels( 
       IntPtr DeviceHandle,
       byte enabledChannels,
       byte channelNumber
    )

    Parameters

    DeviceHandle
    Type: System.IntPtr
    The handle associated with the USB device.
    enabledChannels
    Type: System.Byte
    The enabled channels associated with the USB device.
    The value must be between 0 and 1.
    channelNumber
    Type: System.Byte
    The channel number associated with the USB device.

    Return Value

    Type: System.String
    A value equal to 0; otherwise Error
    Remarks
    The enabledChannels is a value indicating...
    Frameworks
    Product Versions
    .NET net10.0
    .NET Framework net48
    See Also