'DeclarationPublic Function Set_Load_Switch( _ ByVal DeviceHandle As IntPtr, _ ByVal SimulatedLoad As Integer, _ Optional ByVal ChannelNumber As Byte _ ) As String
'UsageDim instance As USB_DLL Dim DeviceHandle As IntPtr Dim SimulatedLoad As Integer Dim ChannelNumber As Byte Dim value As String value = instance.Set_Load_Switch(DeviceHandle, SimulatedLoad, ChannelNumber)
public string Set_Load_Switch( IntPtr DeviceHandle, int SimulatedLoad, byte ChannelNumber )
Parameters
- DeviceHandle
- Type: System.IntPtr
The handle associated with the USB device. - SimulatedLoad
- Type: System.Int32
The simulated load associated with the USB device. - ChannelNumber
- Type: System.Byte
The channel number associated with the USB device.
Return Value
Type: System.String
A value equal to 0; otherwise Error
A value equal to 0; otherwise Error