FUTEK .NET API Documentation
FUTEK_USB_DLL Assembly / FUTEK_USB_DLL Namespace / USB_DLL Class / Set_Number_of_Loading_Points Method
Type: System.IntPtr
The handle associated with the USB device.
Type: System.Int32
The number of calibration loading points associated with the USB device.
The value must be between 0 and 19 (certain models may have fewer loading points).
Type: System.Byte
The channel number associated with the USB device.


In This Topic
    Set_Number_of_Loading_Points Method
    In This Topic
    Warning: The use of this function can affect the factory calibration of the USB device.
    Sets the number of loading point values stored in the EEPROM of the microcontroller.
    Syntax
    'Declaration
     
    
    Public Function Set_Number_of_Loading_Points( _
       ByVal DeviceHandle As IntPtr, _
       ByVal NumberOfLoadingPoints As Integer, _
       Optional ByVal ChannelNumber As Byte _
    ) As String
    'Usage
     
    
    Dim instance As USB_DLL
    Dim DeviceHandle As IntPtr
    Dim NumberOfLoadingPoints As Integer
    Dim ChannelNumber As Byte
    Dim value As String
     
    value = instance.Set_Number_of_Loading_Points(DeviceHandle, NumberOfLoadingPoints, ChannelNumber)
    public string Set_Number_of_Loading_Points( 
       IntPtr DeviceHandle,
       int NumberOfLoadingPoints,
       byte ChannelNumber
    )

    Parameters

    DeviceHandle
    Type: System.IntPtr
    The handle associated with the USB device.
    NumberOfLoadingPoints
    Type: System.Int32
    The number of calibration loading points associated with the USB device.
    The value must be between 0 and 19 (certain models may have fewer loading points).
    ChannelNumber
    Type: System.Byte
    The channel number associated with the USB device.

    Return Value

    Type: System.String
    A value equal to 0; otherwise Error
    Remarks
    The NumberOfLoadingPoints is used to assign the total number of points that are recorded and stored in memory at the time of calibration.
    In order to avoid unexpected behavior, each loading point must have a valid loading point value (ADC Count) and load value (physical load).
    Frameworks
    Product Versions
    .NET net10.0
    .NET Framework net48
    See Also