FUTEK .NET API Documentation
FUTEK_USB_DLL Assembly / FUTEK_USB_DLL Namespace / USB_DLL Class / Set_Sensor_Configuration Method
Type: System.IntPtr
The handle associated with the USB device.
Type: System.Int32
The sensor configuration associated with the USB device.
Type: System.Byte
The channel number associated with the USB device.


In This Topic
    Set_Sensor_Configuration Method
    In This Topic
    Warning: The use of this function can affect the factory calibration of the USB device.
    Sets the sensor configuration stored in the EEPROM of the microcontroller including: Input / Output Type, Nominal Sensitivity and Nominal Bridge Resistance.
    Syntax
    'Declaration
     
    
    Public Function Set_Sensor_Configuration( _
       ByVal DeviceHandle As IntPtr, _
       ByVal SensorConfiguration As Integer, _
       Optional ByVal ChannelNumber As Byte _
    ) As String
    'Usage
     
    
    Dim instance As USB_DLL
    Dim DeviceHandle As IntPtr
    Dim SensorConfiguration As Integer
    Dim ChannelNumber As Byte
    Dim value As String
     
    value = instance.Set_Sensor_Configuration(DeviceHandle, SensorConfiguration, ChannelNumber)
    public string Set_Sensor_Configuration( 
       IntPtr DeviceHandle,
       int SensorConfiguration,
       byte ChannelNumber
    )

    Parameters

    DeviceHandle
    Type: System.IntPtr
    The handle associated with the USB device.
    SensorConfiguration
    Type: System.Int32
    The sensor configuration associated with the USB device.
    ChannelNumber
    Type: System.Byte
    The channel number associated with the USB device.

    Return Value

    Type: System.String
    A value equal to 0; otherwise Error
    Remarks
    Frameworks
    Product Versions
    .NET net10.0
    .NET Framework net48
    See Also