'Declaration
Public Function Set_Type_of_Calibration( _ ByVal DeviceHandle As IntPtr, _ ByVal TypeOfCalibration As Integer, _ Optional ByVal ChannelNumber As Byte _ ) As String
'Usage
Dim instance As USB_DLL Dim DeviceHandle As IntPtr Dim TypeOfCalibration As Integer Dim ChannelNumber As Byte Dim value As String value = instance.Set_Type_of_Calibration(DeviceHandle, TypeOfCalibration, ChannelNumber)
public string Set_Type_of_Calibration( IntPtr DeviceHandle, int TypeOfCalibration, byte ChannelNumber )
Parameters
- DeviceHandle
- Type: System.IntPtr
The handle associated with the USB device. - TypeOfCalibration
- Type: System.Int32
The type of calibration associated with the USB device.
The value must be between 0 and 1. - ChannelNumber
- Type: System.Byte
The channel number associated with the USB device.
Return Value
Type: System.String
A value equal to 0; otherwise Error
A value equal to 0; otherwise Error