'DeclarationPublic Function Set_Unit_Code( _ ByVal DeviceHandle As IntPtr, _ ByVal UnitCode As Integer, _ Optional ByVal ChannelNumber As Byte _ ) As String
'UsageDim instance As USB_DLL Dim DeviceHandle As IntPtr Dim UnitCode As Integer Dim ChannelNumber As Byte Dim value As String value = instance.Set_Unit_Code(DeviceHandle, UnitCode, ChannelNumber)
public string Set_Unit_Code( IntPtr DeviceHandle, int UnitCode, byte ChannelNumber )
Parameters
- DeviceHandle
- Type: System.IntPtr
The handle associated with the USB device. - UnitCode
- Type: System.Int32
The unit code associated with the USB device. - ChannelNumber
- Type: System.Byte
The channel number associated with the USB device.
Return Value
Type: System.String
A value equal to 0; otherwise Error
A value equal to 0; otherwise Error