FUTEK .NET API Documentation
FUTEK_USB_DLL Assembly / FUTEK_USB_DLL Namespace / USB_DLL Class / VirtualSerialNumber Property


In This Topic
    VirtualSerialNumber Property
    In This Topic
    Gets a value indicating the serial number of the virtual USB device.
    Syntax
    'Declaration
     
    
    Public ReadOnly Property VirtualSerialNumber As Integer
    'Usage
     
    
    Dim instance As USB_DLL
    Dim value As Integer
     
    value = instance.VirtualSerialNumber
    public int VirtualSerialNumber {get;}

    Property Value

    Type: System.Int32 The value must be between 0 and System.Int32.MaxValue.
    Remarks
    Frameworks
    Product Versions
    .NET net10.0
    .NET Framework net48
    See Also