'DeclarationPublic Function Write_TEDS_Register( _ ByVal DeviceHandle As IntPtr, _ ByVal HighAddress As Byte, _ ByVal LowAddress As Byte, _ ByVal Data As Byte _ ) As String
'UsageDim instance As USB_DLL Dim DeviceHandle As IntPtr Dim HighAddress As Byte Dim LowAddress As Byte Dim Data As Byte Dim value As String value = instance.Write_TEDS_Register(DeviceHandle, HighAddress, LowAddress, Data)
public string Write_TEDS_Register( IntPtr DeviceHandle, byte HighAddress, byte LowAddress, byte Data )
Parameters
- DeviceHandle
- Type: System.IntPtr
The handle associated with the USB device. - HighAddress
- Type: System.Byte
The high byte of the address associated with the TEDS register. - LowAddress
- Type: System.Byte
The low byte of the address associated with the TEDS register. - Data
- Type: System.Byte
The data to assign the TEDS register.
Return Value
Type: System.String
A value equal to 0; otherwise Error
A value equal to 0; otherwise Error