FUTEK Device Communication

This module provides communication interfaces for FUTEK serial devices.

Custom Exceptions

class futek_device_communication.FutekDeviceError

Bases: Exception

Base exception for all FUTEK device errors

class futek_device_communication.FutekConnectionError

Bases: FutekDeviceError

Raised when connection/disconnection fails

class futek_device_communication.FutekCommunicationError

Bases: FutekDeviceError

Raised when serial communication fails

class futek_device_communication.FutekTimeoutError

Bases: FutekCommunicationError

Raised when a command times out

class futek_device_communication.FutekProtocolError

Bases: FutekDeviceError

Raised when protocol/checksum validation fails

class futek_device_communication.FutekInvalidParameterError

Bases: FutekDeviceError

Raised when invalid parameters are provided

class futek_device_communication.FutekDeviceNotFoundError

Bases: FutekDeviceError

Raised when device discovery fails

class futek_device_communication.FutekCalibrationError

Bases: FutekDeviceError

Raised when calibration data is invalid or missing

FUTEK Serial Scanner

class futek_device_communication.FutekSerialScanner

FUTEKSerialScanner handles discovery operations for FUTEK devices.

classmethod discover_devices(cls, device_models=None, comports=None)

Discovers Futek serial devices.

Parameters:
  • device_models – Device model types to search for.

  • comports – Specific comports to scan.

Returns:

Futek devices discovered during scan.

FUTEK Device

class futek_device_communication.FutekDevice(communication_interface, *, _internal_token=None)

Represents a FUTEK device.

Note

Do not instantiate FutekDevice directly. Use FutekSerialScanner.discover_devices() to obtain FutekDevice instances. Direct instantiation is not supported and will raise TypeError.

Example:
>>> devices = FutekSerialScanner.discover_devices()
>>> if devices:
...     device = devices[0]
disconnect(self)

Disconnects from the FUTEK device.

get_adc_converter(self)
get_adc_for_profile(self, profile_number)
get_auto_teds(self)

Check if AutoTEDS is enabled on the device.

Automatically uses correct command version based on firmware version.

Returns:

True if AutoTEDS enabled, False otherwise

Raises:
  • FutekTEDSNotSupportedError – If device doesn’t support TEDS

  • FutekCommunicationError – If communication fails

get_board_temperature(self)

Gets the board temperature of the device.

Returns:

Device Board Temperature in degrees Celsius.

get_device_channel_selected_profile(self, channel_number=0)

Gets the selected profile number for the specified channel.

Parameters:

channel_number – Channel number to query.

Returns:

Selected profile number as integer.

get_instrument_serial_number(self)

Gets the instrument serial number.

Returns:

Instrument serial number.

get_load_of_loading_point(self, point_index, channel_number=0)

Gets the load value at a specific loading point.

Parameters:
  • point_index – Index of the loading point.

  • channel_number – Channel number to query.

Returns:

Load value as float.

get_loading_point_value(self, point_index, channel_number=0)

Gets the ADC value at a specific loading point.

Parameters:
  • point_index – Index of the loading point.

  • channel_number – Channel number to query.

Returns:

ADC value as integer.

get_model_number(self)

Gets the device model number.

Returns:

Device model number as string.

get_ndr(self, channel_number=0)

Returns normal data request for channel number.

Parameters:

channel_number – Channel number to retrieve data request.

Returns:

ADC value

Raises:

FutekCommunicationError – If communication fails

get_number_of_directions(self, channel_number=0)

Gets the number of load directions for the specified channel.

Parameters:

channel_number – Channel number to query.

Returns:

Number of directions.

get_number_of_loading_points(self, channel_number=0)

Gets the number of loading points for the specified channel.

Parameters:

channel_number – Channel number to query.

Returns:

Number of loading points.

get_reading(self, channel_number=0)

Gets a calibrated reading from the specified channel.

Parameters:

channel_number – Channel number to read from.

Returns:

Calibrated load reading as float.

Raises:
get_sampling_rate(self, channel_number=0)

Gets the current sampling rate for the specified channel.

Parameters:

channel_number – Channel number to query.

Returns:

Current sampling rate.

get_sensor_serial_number(self, channel_number=0)

Gets the sensor serial number for the specified channel.

Parameters:

channel_number – Channel number to query.

Returns:

Sensor serial number.

get_stream_data(self)

Gets raw streaming data from the device buffer.

Returns:

Raw data buffer as bytearray.

get_teds_engineering_unit(self)

Get TEDS engineering unit as a string.

Returns:

Engineering unit string (e.g., “N”, “lb”, “psi”)

Raises:
get_teds_max_capacity(self)

Get TEDS maximum measurement capacity.

Returns:

Maximum capacity in sensor’s native units

Raises:
get_teds_serial_number(self)

Get TEDS sensor serial number.

Returns:

Serial number as string

Raises:
get_teds_template(self)

Get TEDS template/type number.

Returns:

TEDS template number

Raises:
get_unit_of_measure(self, channel_number=0)

Gets the unit of measure for the specified channel.

Parameters:

channel_number – Channel number to query.

Returns:

Unit of measure as UnitOfMeasureEnum.

initialize_teds(self)

Initialize TEDS support during device discovery.

post_teds_operations(self)

Restore device state after TEDS operations.

Restores cached sampling rate and waits for device to stabilize.

Raises:

FutekCommunicationError – If communication fails

pre_teds_operations(self)

Prepare device for TEDS operations.

Caches current sampling rate and sets to lowest rate for reliable TEDS communication.

Raises:

FutekCommunicationError – If communication fails

reload_teds_data(self)

Re-read TEDS data from sensor and update calibration.

This is called automatically when enabling AutoTEDS or can be called manually to refresh TEDS data.

Raises:
  • FutekTEDSNotSupportedError – If device doesn’t support TEDS

  • FutekTEDSNotConnectedError – If no TEDS sensor connected

  • FutekCommunicationError – If communication fails

set_adc_of_loading_point(self, point_index, adc_value, calibration_direction=None, channel_number=0)

Sets the ADC value for a specific loading point.

Parameters:
  • point_index – Index of the loading point.

  • adc_value – ADC value to set.

  • calibration_direction – Calibration direction (reserved for future use).

  • channel_number – Channel number to modify.

Raises:

FutekCommunicationError – If communication fails

set_auto_teds(self, enabled)

Enable or disable AutoTEDS on the device.

When enabling: automatically loads TEDS data and updates calibration. When disabling: reverts to manual calibration from EEPROM.

Parameters:

enabled – True to enable AutoTEDS, False to disable

Raises:
  • FutekTEDSNotSupportedError – If device doesn’t support TEDS

  • FutekCommunicationError – If communication fails

set_device_channel_selected_profile(self, channel_number, profile_number)

Sets the selected profile number for the specified channel.

Parameters:
  • profile_number – Profile number to set.

  • channel_number – Channel number to modify.

set_load_of_loading_point(self, point_index, load_value, channel_number=0)

Sets the load value for a specific loading point.

Parameters:
  • point_index – Index of the loading point.

  • load_value – Load value to set.

  • calibration_direction – Calibration direction (reserved for future use).

  • channel_number – Channel number to modify.

Raises:

FutekCommunicationError – If communication fails

set_number_of_directions(self, number_of_directions, channel_number=0)

Sets the number of load directions for the specified channel.

Parameters:
  • number_of_directions – Number of directions to set.

  • channel_number – Channel number to modify.

set_sampling_rate(self, samples_per_second: Union['USB225SamplingRateEnum', 'QIA128SamplingRateEnum', 'IDC150SamplingRateEnum', 'IEM100SamplingRateEnum'], int channel_number: int = 0) → None

Sets the sampling rate for the specified channel.

Parameters:
  • samples_per_second – Sampling rate enum value to set.

  • channel_number – Channel number to modify.

Raises:

FutekCommunicationError – If communication fails

set_sampling_rate_value(self, samples_per_second, channel_number=0)

Sets the sampling rate for the specified channel.

Parameters:
  • samples_per_second – Sampling rate value to set.

  • channel_number – Channel number to modify.

Raises:

FutekCommunicationError – If communication fails

set_stream_state(self, stream_enabled)

Sets the streaming state for the device.

Parameters:

stream_enabled – True to enable streaming, False to disable.

Raises:

FutekCommunicationError – If communication fails

set_unit_of_measure(self, unit_of_measure, channel_number=0)

Sets the unit of measure for the specified channel.

Parameters:
  • unit_of_measure – Unit of measure enum value to set.

  • channel_number – Channel number to modify.

Raises:

FutekCommunicationError – If communication fails

supports_teds(self)

Check if this device supports TEDS functionality.

Returns:

True if device supports TEDS, False otherwise

teds_is_connected(self)

Check if TEDS sensor is physically connected.

Returns:

True if TEDS sensor is connected, False otherwise

Raises:

If communication fails

ADC Converter

class futek_device_communication.ADCConverter

Converts raw ADC values to calibrated load readings using loading point calibration data.

This class handles the conversion of raw analog-to-digital converter (ADC) values into calibrated engineering units based on device-specific calibration points.

Note

Do not instantiate ADCConverter directly. Use FutekDevice.get_adc_converter() or FutekDevice.get_adc_for_profile() to obtain ADCConverter instances that are properly initialized with calibration data from the device.

TEDS Data

Note

TEDS properties should be accessed through the FutekDevice class methods.

TEDS Initialization Example

The following example demonstrates how to properly initialize TEDS (Transducer Electronic Data Sheet) data and retrieve TEDS information from a device:

 1def teds_scaled_reading():
 2    futek_devices = FutekSerialScanner.discover_devices()
 3    device: FutekDevice = futek_devices[0]
 4    device.pre_teds_operations()
 5    device.initialize_teds()
 6    device.post_teds_operations()
 7
 8    reading = device.get_reading()
 9
10    print(f"teds is connected: {device.teds_is_connected()}")
11    print(f"teds template: {device.get_teds_template()}")
12    print(f"teds serial number: {device.get_teds_serial_number()}")
13    print(f"teds engineering unit: {device.get_teds_engineering_unit()}")
14    print(f"teds max capacity: {device.get_teds_max_capacity()}")
15    print(f"auto teds enbaled {device.get_auto_teds()}")

Key Steps:

  1. Discover devices - Use FutekSerialScanner.discover_devices() to find connected devices

  2. Pre-TEDS operations - Call device.pre_teds_operations() to prepare the device

  3. Initialize TEDS - Call device.initialize_teds() to load TEDS data

  4. Post-TEDS operations - Call device.post_teds_operations() to complete initialization

  5. Access TEDS data - Use FutekDevice getter methods to retrieve TEDS information

Available TEDS Methods on FutekDevice:

  • device.teds_is_connected() - Check if TEDS is connected

  • device.get_teds_template() - Get template identifier

  • device.get_teds_serial_number() - Get TEDS serial number

  • device.get_teds_engineering_unit() - Get engineering unit

  • device.get_teds_max_capacity() - Get maximum capacity

  • device.get_auto_teds() - Check if auto-TEDS is enabled

Stream Data Converter

class futek_device_communication.StreamReading(calibrated_value, adc_value)

Single reading from stream data.

adc_value

adc_value: ‘unsigned long’

calibrated_value

calibrated_value: ‘double’

class futek_device_communication.StreamConversionResult(readings, remainder)

Result from stream data conversion.

readings

readings: list

remainder

remainder: bytearray

class futek_device_communication.StreamDataConverter

Utility class for converting raw streaming data into calibrated readings.

Provides methods to parse and validate streaming data packets from FUTEK devices, converting raw byte streams into tuples of (calibrated_reading, adc_value). Implements checksum validation to detect corrupted packets and handles partial data buffers for continuous streaming operations.

static convert_stream_data_to_reading(data, adc_converter)

Convert stream data with validation and error logging.

Parameters:
  • data – Raw stream data

  • adc_converter – ADC converter instance or callable

Returns:

StreamConversionResult containing readings and remainder bytes

static convert_stream_data_to_reading_38_kHz(data, adc_converter)

Convert stream data for USB225 at 38.4kHz with validation and error logging.

Parameters:
  • data – Raw stream data

  • adc_converter – ADC converter instance or callable

Returns:

StreamConversionResult containing readings and remainder bytes

Unit of Measure Enum

class futek_device_communication.UnitOfMeasureEnum(*values)

Available units of measure for FUTEK devices.

Supports various measurement units including: - Force: lb, N, kg, oz, gram, dyn, kN, mN - Torque: Nm, Ncm, Nmm, inch_lb, inch_oz, ft_lb, kg_cm, kg_m, kNm - Pressure: psi, bar, Pa, kPa, MPa, atm, mbar, mm_Hg, inch_H2O, ft_H2O - Distance: mm, cm, dm, m, km, inch, ft, yd, mi - Temperature: C, F, K, Ra - Electrical: V, mV, uV, nV, kV, A, mA, uA, mVV, Ohms - Mass: g, mg, ug, kg, MT, ST, LT

Sampling Rate Enums

USB225 Sampling Rates

class futek_device_communication.USB225SamplingRateEnum(*values)

Sampling rates available for USB225 devices.

Supports rates from 2.5 SPS to 38,400 SPS.

Note: The 38,400 SPS rate (SPS_38400) is only available on USB225 Pro Elite.

Available rates: 2.5, 5, 10, 16.6, 20, 50, 60, 100, 400, 1200, 2400, 4800, 7200, 14000, 19200, 38400 samples per second.

Example Usage:

from futek_device_communication import USB225SamplingRateEnum

# Set sampling rate to 100 SPS
device.set_sampling_rate(USB225SamplingRateEnum.SPS_100)

# Set sampling rate to 2400 SPS
device.set_sampling_rate(USB225SamplingRateEnum.SPS_2400)

QIA128 Sampling Rates

class futek_device_communication.QIA128SamplingRateEnum(*values)

Sampling rates available for QIA128 devices.

Supports rates from 4 SPS to 1300 SPS.

Available rates: 4, 20, 50, 100, 200, 500, 850, 1300 samples per second.

Example Usage:

from futek_device_communication import QIA128SamplingRateEnum

# Set sampling rate to 100 SPS
device.set_sampling_rate(QIA128SamplingRateEnum.SPS_100)

# Set sampling rate to 500 SPS
device.set_sampling_rate(QIA128SamplingRateEnum.SPS_500)

IDC150 Sampling Rates

class futek_device_communication.IDC150SamplingRateEnum(*values)

Sampling rates available for IDC150 devices.

Supports rates from 4 SPS to 1300 SPS.

Available rates: 4, 20, 50, 100, 200, 500, 850, 1300 samples per second.

Example Usage:

from futek_device_communication import IDC150SamplingRateEnum

# Set sampling rate to 100 SPS
device.set_sampling_rate(IDC150SamplingRateEnum.SPS_100)

# Set sampling rate to 850 SPS
device.set_sampling_rate(IDC150SamplingRateEnum.SPS_850)

IEM100 Sampling Rates

class futek_device_communication.IEM100SamplingRateEnum(*values)

Sampling rates available for IEM100 devices.

Supports rates from 4 SPS to 1300 SPS.

Available rates: 4, 20, 50, 100, 200, 500, 850, 1300 samples per second.

Example Usage:

from futek_device_communication import IEM100SamplingRateEnum

# Set sampling rate to 100 SPS
device.set_sampling_rate(IEM100SamplingRateEnum.SPS_100)

# Set sampling rate to 850 SPS
device.set_sampling_rate(IEM150SamplingRateEnum.SPS_850)