FUTEK .NET API Documentation
FUTEK.Devices Assembly / FUTEK.Devices Namespace / Device Class / Equals Method / Equals(Device) Method


In This Topic
    Equals(Device) Method
    In This Topic
    Determines whether the specified device is equal to the current device instance.
    Syntax
    'Declaration
     
    
    Public Overloads Function Equals( _
       ByVal x As Device _
    ) As Boolean
    'Usage
     
    
    Dim instance As Device
    Dim x As Device
    Dim value As Boolean
     
    value = instance.Equals(x)
    public bool Equals( 
       Device x
    )

    Parameters

    x

    Return Value

    True if the specified device is equal to the current device instance, otherwise false.
    Frameworks
    Product Versions
    .NET net10.0
    .NET Framework net48
    See Also