FUTEK .NET API Documentation
FUTEK.Devices Assembly / FUTEK.Devices Namespace / LoadingPoint Class / Inequality Operator


In This Topic
    Inequality Operator
    In This Topic
    Determines whether two specified instances of LoadingPoint are not equal.
    Syntax
    'Declaration
     
    
    Public Operator <>( _
       ByVal lhs As LoadingPoint, _
       ByVal rhs As LoadingPoint _
    ) As Boolean
    'Usage
     
    
    public bool operator !=( 
       LoadingPoint lhs,
       LoadingPoint rhs
    )

    Parameters

    lhs
    rhs

    Return Value

    true if lhs and rhs do not represent the same LoadingPoint; otherwise, false.
    Frameworks
    Product Versions
    .NET net10.0
    .NET Framework net48
    See Also