'Declaration
Public Function Set_Voltage_Output( _ ByVal DeviceHandle As IntPtr, _ ByVal VoltageOutput As Integer, _ Optional ByVal ChannelNumber As Byte _ ) As String
'Usage
Dim instance As USB_DLL Dim DeviceHandle As IntPtr Dim VoltageOutput As Integer Dim ChannelNumber As Byte Dim value As String value = instance.Set_Voltage_Output(DeviceHandle, VoltageOutput, ChannelNumber)
public string Set_Voltage_Output( IntPtr DeviceHandle, int VoltageOutput, byte ChannelNumber )
Parameters
- DeviceHandle
- Type: System.IntPtr
The handle associated with the USB device. - VoltageOutput
- Type: System.Int32
The voltage output associated with the USB device. - ChannelNumber
- Type: System.Byte
The channel number associated with the USB device.
Return Value
Type: System.String
A value equal to 0; otherwise Error
A value equal to 0; otherwise Error