FUTEK .NET API Documentation
FUTEK_USB_DLL Assembly / FUTEK_USB_DLL Namespace / USB_DLL Class / Set_Baud_Rate Method
Type: System.IntPtr
The handle associated with the USB device.
The Baud rate value associated with the USB device.
The value must be between 0 and 3.
Type: System.Byte
The channel number associated with the USB device.


In This Topic
    Set_Baud_Rate Method
    In This Topic
    Warning: The use of this function can affect the factory calibration of the USB device.
    Sets the Baud rate value stored in the EEPROM of the microcontroller.
    Syntax
    'Declaration
     
    
    Public Function Set_Baud_Rate( _
       ByVal DeviceHandle As IntPtr, _
       ByVal BaudRate As Integer, _
       Optional ByVal ChannelNumber As Byte _
    ) As String
    'Usage
     
    
    Dim instance As USB_DLL
    Dim DeviceHandle As IntPtr
    Dim BaudRate As Integer
    Dim ChannelNumber As Byte
    Dim value As String
     
    value = instance.Set_Baud_Rate(DeviceHandle, BaudRate, ChannelNumber)

    Parameters

    DeviceHandle
    Type: System.IntPtr
    The handle associated with the USB device.
    BaudRate
    The Baud rate value associated with the USB device.
    The value must be between 0 and 3.
    ChannelNumber
    Type: System.Byte
    The channel number associated with the USB device.

    Return Value

    Type: System.String
    A value equal to 0; otherwise Error
    Remarks
    The BaudRate is a value that represents the Baud rate expressed in bits per second.
    Frameworks
    Product Versions
    .NET net8.0
    .NET Framework net48
    See Also