'DeclarationPublic Function Set_Calibration_Code( _ ByVal DeviceHandle As IntPtr, _ ByVal CalibrationCode As Integer, _ Optional ByVal ChannelNumber As Byte _ ) As String
'UsageDim instance As USB_DLL Dim DeviceHandle As IntPtr Dim CalibrationCode As Integer Dim ChannelNumber As Byte Dim value As String value = instance.Set_Calibration_Code(DeviceHandle, CalibrationCode, ChannelNumber)
public string Set_Calibration_Code( IntPtr DeviceHandle, int CalibrationCode, byte ChannelNumber )
Parameters
- DeviceHandle
- Type: System.IntPtr
The handle associated with the USB device. - CalibrationCode
- Type: System.Int32
The calibration code associated with the USB device.
The value must be between 0 and 255. - ChannelNumber
- Type: System.Byte
The channel number associated with the USB device.
Return Value
Type: System.String
A value equal to 0; otherwise Error
A value equal to 0; otherwise Error