'DeclarationPublic Function Set_Calibration_Year( _ ByVal DeviceHandle As IntPtr, _ ByVal CalibrationYear As Integer, _ Optional ByVal ChannelNumber As Byte _ ) As String
'UsageDim instance As USB_DLL Dim DeviceHandle As IntPtr Dim CalibrationYear As Integer Dim ChannelNumber As Byte Dim value As String value = instance.Set_Calibration_Year(DeviceHandle, CalibrationYear, ChannelNumber)
public string Set_Calibration_Year( IntPtr DeviceHandle, int CalibrationYear, byte ChannelNumber )
Parameters
- DeviceHandle
- Type: System.IntPtr
The handle associated with the USB device. - CalibrationYear
- Type: System.Int32
The calibration day associated with the USB device.
The value must be between 0 and 255. - ChannelNumber
- Type: System.Byte
The channel number associated with the USB device.
Return Value
Type: System.String
A value equal to 0; otherwise Error
A value equal to 0; otherwise Error