FUTEK .NET API Documentation
FUTEK_USB_DLL Assembly / FUTEK_USB_DLL Namespace / USB_DLL Class / Set_Calibration_Day Method
Type: System.IntPtr
The handle associated with the USB device.
Type: System.Int32
The calibration day associated with the USB device.
The value must be between 1 and 31.
Type: System.Byte
The channel number associated with the USB device.


In This Topic
    Set_Calibration_Day Method
    In This Topic
    Warning: The use of this function can affect the factory calibration of the USB device.
    Sets the calibration day stored in the EEPROM of the microcontroller.
    Syntax
    'Declaration
     
    
    Public Function Set_Calibration_Day( _
       ByVal DeviceHandle As IntPtr, _
       ByVal CalibrationDay As Integer, _
       Optional ByVal ChannelNumber As Byte _
    ) As String
    'Usage
     
    
    Dim instance As USB_DLL
    Dim DeviceHandle As IntPtr
    Dim CalibrationDay As Integer
    Dim ChannelNumber As Byte
    Dim value As String
     
    value = instance.Set_Calibration_Day(DeviceHandle, CalibrationDay, ChannelNumber)
    public string Set_Calibration_Day( 
       IntPtr DeviceHandle,
       int CalibrationDay,
       byte ChannelNumber
    )

    Parameters

    DeviceHandle
    Type: System.IntPtr
    The handle associated with the USB device.
    CalibrationDay
    Type: System.Int32
    The calibration day associated with the USB device.
    The value must be between 1 and 31.
    ChannelNumber
    Type: System.Byte
    The channel number associated with the USB device.

    Return Value

    Type: System.String
    A value equal to 0; otherwise Error
    Remarks
    The CalibrationDay is a value representing the day of the month when calibration of the USB device was performed.
    Frameworks
    Product Versions
    .NET net10.0
    .NET Framework net48
    See Also