This table provides a comprehensive list of commands and the response of each command. The responses have been separated for commands that were successful and unsuccessful. If the command was sent and received successfully, then the response will typically be either 0 or a number in a given range. Please refer to the sections related to a specific command for more information. If the command was sent and received unsuccessfully, then the response will be “Error” and the ErrorDescription will be updated. Please refer to the Common Command Errors or Specific Command Errors for more information.
This table provides a comprehensive list of commands and the specific command errors that can be returned by the ErrorDescription when a command is unsuccessful.